Southco Resource Center

유익한 글, 자료, 동영상 등 각종 콘텐츠를 이용하고 공유해주세요.

The Importance of Material Selection in Compression Latches for Harsh Environments

July 24 2025
The Importance of Material Selection in Compression Latches for Harsh Environments

Compression latches are an essential component of many industrial and commercial applications, providing secure and reliable fastening between a panel and frame. However, not all compression latches are created equal, and the material selection plays a critical role in their performance when they are exposed to harsh environments.
These environments, such as those with high levels of humidity, temperature fluctuations, corrosive chemicals, and abrasive particles can significantly impact the performance of compression latches. In these conditions, selecting the right materials for the latch becomes even more critical.


The following are some key factors that design engineers should consider when selecting materials for compression latches used in harsh environments.

  1. Corrosion Resistance - Corrosion is a common problem in harsh environments, and it can accelerate performance decline that can ultimately led to hardware failure. Therefore, design engineers should select materials that have high corrosion resistance, such as stainless steel, aluminum, or plastic. Stainless steel is an excellent choice because it offers excellent corrosion resistance and durability.
  2. Temperature Resistance - Temperature fluctuations can cause compression latches to expand or contract, affecting their fit and function. Therefore, design engineers should select materials that have good temperature resistance, such as high-temperature plastics or metals like stainless steel or aluminum. They should also consider the maximum and minimum temperatures that the latch will be exposed to and select the appropriate material accordingly.
  3.  Impact Resistance - Compression latches may be subject to impacts and vibration, which can cause them to break or malfunction. Choosing materials that can withstand these hits and rattles, such as reinforced plastics or metals like steel or aluminum, is critical. They should also consider the maximum force of impact that the latch may be subject to and select the appropriate material accordingly.
  4. Chemical Resistance – Some devices may need to function in environments with corrosive chemicals that can damage compression latches. In these situations, engineers should select materials that have good chemical resistance, such as plastics or metals that are resistant to the specific chemicals present in the environment.
    Selecting the right materials for compression latches is crucial to their performance and longevity in certain situations. Design engineers should consider the unique requirements of the environment and select materials that have high corrosion resistance, temperature resistance, impact resistance, and chemical resistance. By doing so, they can ensure that the compression latch they choose will provide reliable and secure fastening in even the harshest environments.

Selecting the right materials for compression latches is crucial to their performance and longevity in certain situations. Design engineers should consider the unique requirements of the environment and select materials that have high corrosion resistance, temperature resistance, impact resistance, and chemical resistance. By doing so, they can ensure that the compression latch they choose will provide reliable and secure fastening in even the harshest environments.