Southco’s Software Development Kit (SDK) contains a set of tools that makes it easy to communicate with Southco Bluetooth® enabled devices.
The SDK supports app development using the React Native framework and can be used as a guide when developing native apps.
Requirements: The Southco Bluetooth controllers must be unregistered in their factory default state and using the latest revision of the device firmware.The Southco Utility App (available on the Apple App Store and Google Play Store ) can be used to confirm the firmware revision and perform an update if required.